Details
An Interpart Copy of a part, with some colored faces, will not update if colors
are changed in the source part. Even 'Recompute' or 'Update Link' will keep the
previous colors.
Solution
The user has to clear all colors before updating. Use 'Part Painter' to apply
style '(none)' to the 'Feature' Part Copy option 'Replace Styles'. This will
reset the Part Copy to the default color.
Afterwards doing a 'Recompute' or 'Update Link' on the Part Copy will get the
latest colors from the basic part.
Notes and References
PR#7961848
Hardware/Software Configuration
Platform: INTEL
OS: window
OS Version: 864
Product: SOLID_EDGE
Application: ASSEMBLY
Function: DISPLAY
Ref: 002-7009080