The Member Select and Preview are missing from the Reuse Library dialog,
preventing the selection of a Reuse Library object. This could be also seen in
the part navigator and Assembly Navigator that the Details, Dependencies, and
Previews are missing from the Navigators pane at the bottom.
Solution
This is most likely due to a corrupt NX registry. To correct this, shut down
NX. Use the Windows Regedit command to edit the Windows Registry. In the
Windows Registry Editor, select and expand:
HKEY_CURRENT_USER\Software\Unigraphics Solutions\NX
Delete the 13.0 folder (or the appropriate version of NX that is exhibiting
this behavior).

Restarting NX will recreate this Registry Key and the issue should be resolved.
Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 1064
Product: NX
Application: KDA
Version: V1847
Function: REUSE_LIBRARY
Ref: 002-7009079