When creating new features with a boolean operation, the feature is not getting
set to the correct color.
Solution
There are two preferences that define the feature colors:
Preferences -> Object, and edit the "Solid Body" color to something other than
what is currently set.

Preferences -> Modeling, and edit the "New Face Properties" to "Part Default".

Select the correct options to what you want as the results.
Notes and References
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: GATEWAY
Version: V1847
Function: PREFERENCES
Ref: 002-7009078