NX After Installing NX, Progressive Die Wizard Standard Parts are Missing

2021-10-06T23:26:56Z
NX for Design

Summary


Details

--------------- 
After installing NX, the Progressive Die Wizard Standard Parts are missing.



Solution

The NX install does not include the Progressive Die Wizard Standard Parts because of the 
size of the library. An additional download is required and then that ZIP file 
must be uncompressed and installed.


The ZIP file needed can be found at the following location:

NX -> NX -> NX 1847 Series -> Add Ons -> Progressive Die Wizard, look for the file with Data Zip in the file name and extension.

Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: KDA
Version: V1847
Function: PROGRESSIVE_DIE

Ref: 002-7009035

KB Article ID# PL7009035

Contents

SummaryDetails

Associated Components

Tooling Design