NX After Installing NX, Mold Wizard Standard Parts are Missing

2021-10-06T23:26:53Z
NX for Design

Summary


Details

After installing NX, the Mold Wizard Standard Parts are missing.



Solution

 The NX install does not include the Mold Wizard Standard Parts because of the 
size of the library. An additional download is required and then that ZIP file 
must be uncompressed and installed.


The ZIP file needed can be found at the following location:

NX -> NX -> NX 1847 Series -> Add Ons -> Mold Wizard, look for the file with Data Zip in the file name and extension.

Notes and References


Hardware/Software Configuration

Platform: all
OS: all
OS Version: n/a
Product: NX
Application: KDA
Version: V1847
Function: MOLDWIZARD

Ref: 002-7009034

KB Article ID# PL7009034

Contents

SummaryDetails

Associated Components

Tooling Design