NX View Representation column is not available in the Part Navigator

2021-10-06T23:26:48Z
NX for Design

Summary


Details

The 'View Representation' column is not available in the Part Navigator. 
Specifically this column may be needed to see the 'Snapshot' icon in the 
column.


For example: 'Snapshot' is turned ON for one of the drawing views. 
The Snapshot icon can be denoted in the 'View Representation' column of the 
Part Navigator. But the 'View Representation' is missing in the list as an 
available column to be added to the Part Navigator.



Solution

 This column is not available in base NX10.0.0. 
Upgrade to the latest maintenance release and maintenance pack of NX10 to have 
the 'View Representation' available as a column in the Part Navigator.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V10.0
Function: DRAWING/VIEW

Ref: 002-7008979

KB Article ID# PL7008979

Contents

SummaryDetails

Associated Components

Drafting