Solid Edge Split Face command ignores multiple selection using fence select

2021-10-06T23:55:35Z
PART/SHEETMETAL

Summary


Details

Using "Split Face", and then selecting multiple sketch elements using fence 
select will only highlight one element for splitting and ignore all others. 
No error message or other indication of what went wrong is shown.



Solution

Check whether the base coordinate-system is shown, which will then also be 
selected by the fence select and causes the "Split Face" to fail.


Try the following workarounds:


1. Disable or hide all elements which should not be used for splitting. 
2. Alternatively select every sketch element individually. 
3. Otherwise deselect the base-coordinate system after doing the fence select.



Notes and References

PR#8327065



Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 864
Product: SOLID_EDGE
Application: PART/SHEETMETAL
Function: FEATURES

Ref: 002-7008967

KB Article ID# PL7008967

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FLAT_PATTERN