No icons

2021-10-07T00:01:38Z

Summary


Details

There are no icons on the standard or ribbon style UI.



Solution

You can see: File | Edit | View | Modeling | Kinematics | Operations | Weld | Robotics | CEE | Human | Tools | Help


The boxes under have no icons. Empty areas where the icons should be. 
With some laptops like HP, there is an option in the video screen resolution to change the size of the video from 100%, 125%, 150%. 
Make sure the video is at 100%. Anything else will give you empty icons.


Another Icon problem. Totally different from the one listed above is where the only icon options listed are under the Customize menu. 
The only options available are "Menu Bar" or "Standard". Everything else is not available. 

You need to do, step by step: 
  • Make sure Process Simulate is working. 
  • Exit Process Simulate. 
  • Start Tecnomatix Doctor. 
  • Turn off Welcome. 
  • Start Process Simulate. Make sure it still works. 
  • Close Process Simulate. 
  • Open Tecnomatix Doctor. 
  • Turn off Ribbon Style UI. 
  • Enable Roaming OFF.


Icons should be back.



Notes and References


Hardware/Software Configuration

Platform: na
OS: n/a
OS Version: n/a
Product: TECNOMATIX
Application: PROCESS_SIMULAT
Version: V14.0
Function: API

Ref: 002-7008965

KB Article ID# PL7008965

Contents

SummaryDetails

Associated Components