NX CMM Inspection does not allow an edge to be selected when using
Features -> MB3 -> Insert -> Edge Point. What could be preventing this?

Solution
If the
Point on Curve option is disabled on the
Selection Bar then it will not be possible to pick an edge on the model. The
Point on Curve option can be see in the picture below. The menu seen below is displayed when
Mouse Button Three is pressed in the graphics window.

The
Point on Curve option can also be enabled on the
Selection Bar as seen below.

Notes and References
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CMM_INSPECTION
Version: V1880
Function: FEATURES
Ref: 002-7008951