Tecnomatix RCS vs. OLP

2021-10-07T00:01:42Z
Process Simulate

Summary


Details

What can be done with RCS that cannot be done with OLP?



Solution

RCS allows accurate cycle time and trajectory planning. Using OLP only gives you the internal motion planning, which is likely not an accurate cycle time, nor is the trajectory planning specific to the robot manufacturer. Also, OLP downloads may not be correct, because the taught positions possibly could have 
the wrong configuration strings.



Notes and References


Hardware/Software Configuration

Platform: na
OS: n/a
OS Version: n/a
Product: TECNOMATIX
Application: PROCESS_SIMULAT
Version: V13.0
Function: ROBOTICS

Ref: 002-7008948

KB Article ID# PL7008948

Contents

SummaryDetails

Associated Components

Robotics & Automation Shopfloor