Simcenter 3D Solutions Export Material to Library has moved in NX11

2021-10-06T23:26:52Z
Simcenter 3D

Summary


Details

--------------- 

Export Material to Library is not found in NX11 when using 

Manage Library Materials

Solution

 Starting NX11, the dialog box has changed.

In NX10 after starting Export Material to Library you had direct access to 

Export Material to Library 

Edit Library Material 

Delete Material From Library

In NX11, these options are accessible via Right Mouse Button after 

selecting the Material.

A detailed description of the functionality can be found here:

https://docs.plm.automation.siemens.com/tdoc/nx/11.0.1/nx_help/#uid:xid1070457

Notes

KB Article ID# PL7008946

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow