AutoCAD wizard will not appear when Options is selected?

2021-10-06T23:55:19Z

Summary


Details

AutoCAD wizard will not appear when Options is selected?



Solution

 The seacad.ini file was manually edited and the user was not able to save the file. The file was moved to the appdata folder. Once the seacad.ini that was in the appdata folder was removed, the AutoCAD wizard appeared.



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 10_1809
Product: SOLID_EDGE
Application: TRANSLATORS
Version: V220.0
Function: AUTOCAD

Ref: 002-7008938

KB Article ID# PL7008938

Contents

SummaryDetails

Associated Components