How do you place a drawing view of a flat pattern?
Solution
While placing the Drawing View in Draft, click on the Drawing View Wizard Options button on the command bar, then select the Flat pattern radial button from the dialog. It should also be noted that a Flat Pattern needs to be created in the Sheetmetal file first.
Notes and References
Hardware/Software Configuration
Platform: INTEL
OS: windows
OS Version: 10_1809
Product: SOLID_EDGE
Application: DRAFT
Version: V220.0
Function: DRAWING_VIEWS
Ref: 002-7008933