Parts disappear when zooming in and out of assembly

2021-10-06T23:55:26Z

Summary


Details

While zooming in and out of an assembly many parts are disappearing. The user 
checked 'Culling' in Solid Edge Options is turned off - but any change of 
culling does not change the result.



Solution

 Open the assembly and select Control+Shift+F5 from the keyboard - this will 
initiate a rebuild of the geometry caches and restore the expected display. 
This might take a few seconds with a large file, and the file will need to be 
saved after doing the Control+Shift+F5 to eliminate the bad caches.


The user will have to determine which file might contain the bad caches. 
In most cases it is the top assembly file (usually containing assembly 
features or pipes/tubes etc.). However some of the duplicates may have at 
least one subassembly and one part document with the problem.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: n/a
Product: SOLID_EDGE
Application: ASSEMBLY
Function: DISPLAY

Ref: 002-7008926

KB Article ID# PL7008926

Contents

SummaryDetails

Associated Components