Solid Edge Assembly Driven Part Feature does not cut all parts

2021-10-06T23:55:28Z
ASSEMBLY

Summary


Details

I have an assembly in which I want to create an Assembly Driven Part Feature 
which I want to cut through all parts. However there are parts in the assembly 
which are not cut. Why?



Solution

 Check the parts which are not being cut - do they already have inter-part links 
to a different in-context assembly?


When creating Assembly Driven Part Features inter-part links are defined to the 
assembly that creates the Assembly Driven Part Feature. This is not possible if 
the part already has inter-part links with a different in-context assembly and 
thus will explain why you cannot create the Assembly Driven Part Features to a 
new assembly.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: n/a
Product: SOLID_EDGE
Application: ASSEMBLY
Function: FEATURES

Ref: 002-7008921

KB Article ID# PL7008921

Contents

SummaryDetails

Associated Components

ASSEMBLY: ANNOTATIONS/DIMENSIONS