Problems with defining multiple PAX preferences in Teamcenter

2021-10-06T23:26:50Z

Summary


Details

--------------- 
Problems with defining multiple PAX preferences in Teamcenter


Set the preference TC_NX_FileNewPAXFiles_NX11 to the item revision containing 
the modeling pax file and the item revision containing the drafting pax file 
TC_NX_FileNewPAXFiles_NX11=000108/A, 000109/A.


The pax files in Teamcenter are ignored and NX now shows information from the 
native pax file. 
How do you define the multiple pax files?



Solution

 In Teamcenter RAC 
Edit - Options - Search - TC_NX_FileNewPAXFiles_NX11 
Current setup: 
using Single for Multiple section 
TC_NX_FileNewPAXFiles_NX11=000108/A, 000109/A 


Solution: 
Define using the Multiple Option for Multiple(Defines if several values can be 
given for a preference instance). Typically there are multiple values, such as 
one for the model PAX file, one for the drawing PAX file, and so on.


Multiple Values will most likely be set to True (unless only one PAX file will 
be used).


TC_NX_FileNewPAXFiles_NX11= 
Values 
000600/A 
000601/A



Notes and References

IR 7944663



Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 764sp1
Product: NX
Application: NXMANAGER
Version: V11.0
Function: FILE_NEW

Ref: 002-7008918

KB Article ID# PL7008918

Contents

SummaryDetails

Associated Components