Solid Edge Broken out Section View failing

2021-10-06T23:55:16Z
DRAFT

Summary


Details

'Broken-Out' Section View in draft is failing at a specific depth with error 
message.



Solution

It is not known why this may occur and the following suggestions may not 
succeed in every case but are worth a try:


1. First create a Broken-Out Section View, using a depth which will work 
(e.g. through the whole assembly/part) 
2. Then change the depth to the depth which was failing before and see if the 
issue has been cleared. 
3. If these steps worked, you may delete the existing Broken-Out section view, 
and create a new one, using the 'problematic' depth directly. 
4. You can even close the drawing without saving, and create a new (identical) 
Broken-Out section view again without errors.



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 864
Product: SOLID_EDGE
Application: DRAFT
Function: DRAWING_VIEWS

Ref: 002-7008872

KB Article ID# PL7008872

Contents

SummaryDetails

Associated Components

DRAFT: DRAWING_VIEWS