Opening options dialog in legacy STEP translator throws error

2021-10-06T23:55:25Z

Summary


Details

Enabling the legacy STEP translator in ST9 by setting a Registry key may throw 
an error if the "Options" button is used while exporting a STEP file.


The legacy STEP translator should not be used in ST9, however it will work, and 
there are occasions when you have to use it.


The error is shown after following steps:


1. Activate old STEP translator from ST8 in the registry: HKEY-CURRENT_USER - 
SOFTWARE - Unigraphic Solutions - Solid Edge - Version 109 - DEBUG, DWORD 
UselegacySTEPtranslator = 1. 
2. Return to your file and do a 'save as' and choose STEP. 
3. Click "Options" 
4. You will get an error retrieving STEP options.



Solution

The reason for this is likely to be that "STEP3D.INI" is missing. To resolve 
this issue you will need to copy this file from the ST8 installation to 
"..\Solid Edge ST9\Preferences\Translators".



Notes and References

IR#8324915



Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 864
Product: SOLID_EDGE
Application: TRANSLATORS
Function: STEP

Ref: 002-7008870

KB Article ID# PL7008870

Contents

SummaryDetails

Associated Components