Solid Edge Cannot use a propseed.txt file with the Author property

2021-10-06T23:55:06Z
PART/SHEETMETAL

Summary


Details

Trying to create a selectable list of Author names for the Author property on the Solid Edge file properties by defining an entry in propseed.txt file.  However this is not working.  Why?



Solution

The Author property is a Solid Edge system property that is tied to the Windows profile user id.  Therefore this value cannot be changed.  Because the value is tied to the system and cannot be changed, then creating a propseed.txt file to change this system property value will not work.

Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: APPLICATION
Version: V219.0
Function: PROPERTIES

Ref: 002-7008859

KB Article ID# PL7008859

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FEATURES