Solid Edge Changing the default value for the Author property

2021-10-06T23:55:23Z
PART/SHEETMETAL

Summary


Details

How to change or define the default value for the Author property on the Solid Edge file properties?



Solution

The Author property is a Solid Edge system property that is tied to the Windows profile user id. Therefore this value cannot be changed unless the Windows profile user id value is changed. 


The workaround is to create a custom property to use for tracking any required Author detail.

Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: APPLICATION
Version: V219.0
Function: PROPERTIES

Ref: 002-7008858

KB Article ID# PL7008858

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FEATURES