Middle mouse button not rotating geometry

2021-10-06T23:55:33Z

Summary


Details

The middle mouse button is not behaving as expected and is *not* rotating the Solid Edge model as expected.



Solution

The behaviour of the middle mouse button in Solid Edge is controlled by the mouse settings at the operating system level.


The user must explicitly configure/define the mouse property settings to have the middle mouse button configured as a "middle button". If the user has configured the middle mouse button for some other function other than "middle button" then the middle button in Solid Edge will *not* behave as expected 
and cannot be used for rotating in Solid Edge.

Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: APPLICATION
Version: V219.0
Function: OTHER

Ref: 002-7008856

KB Article ID# PL7008856

Contents

SummaryDetails

Associated Components