Solid Edge True Type font not appearing in Solid Edge dialogues

2021-10-06T23:55:18Z
PART/SHEETMETAL

Summary


Details

After adding a True Type font to the Windows font folder, the font is not listed as a selectable option in the various Solid Edge dialogs using fonts.  Why?



Solution

Solid Edge requires True Type fonts to be marked "Installable".  If the font is marked as anything else e.g. "Editable", Solid Edge will not be able to use the font.


If you require using a specific font with Solid Edge that is currently not marked as "Installable", you will need to contact the author of the font and request the font be marked as "Installable" - typically this requires purchasing of the font.

Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: APPLICATION
Version: V219.0
Function: OTHER

Ref: 002-7008855

KB Article ID# PL7008855

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FEATURES