Free Viewer shortcut missing with ST9 MP1 and later

2021-10-06T23:55:32Z

Summary


Details

After installing ST9 MP1 or later, there is no shortcut provided to the free Viewer.



Solution

With base ST9, we inadvertently did not install the free Viewer with the core Solid Edge install. Just as with previous versions, you cannot install the Viewer as a separate product when Solid Edge is already 
installed. Therefore with ST9 there is no way to install the Viewer separately. With ST9 MP1 and later we provided the Viewer .exe as part of the Solid Edge maintenance pack installation. However, because of the 
nature of the MP technology, there is no way to provide a Start menu shortcut for the now provided ST9 Viewer.


With ST9 MP1 or later installed, you will need to manually create a shortcut for all users to the Solid Edge Viewer .exe file:


1. In "C:\ProgramData\Microsoft\Windows\Start Menu\Programs\Solid Edge ST9" create a new Shortcut.


2. Point the Shortcut to "C:\Program Files\Solid Edge ST9\Program\win32\seviewer.exe".


3. Name the Shortcut "Solid Edge Viewer ST9".


With ST9 MP1 and higher installed, following the above instructions will resolve the missing Viewer shortcut issue.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764
Product: SOLID_EDGE
Application: INSIGHT_CONNECT
Version: V219MP1
Function: FREE_VIEWER

Ref: 002-7008853

KB Article ID# PL7008853

Contents

SummaryDetails

Associated Components