Solid Edge free viewer is no longer available with ST9

2021-10-06T23:55:08Z

Summary


Details

After installing ST9, the free viewer is no longer installed by default with ST9.  If you try to install the free viewer alongside Solid Edge, the installation is blocked because Solid Edge is already installed.



Solution

With previous versions of Solid Edge the free viewer was always installed automatically as part of the core Solid Edge install.  The Viewer could never be installed as a separate product.


In ST9, inadvertently the free viewer was not installed with the core Solid Edge install.  Just as with previous versions, you cannot install the viewer as a separate product when Solid Edge is already installed. 
Therefore with ST9 there is no way to install the Viewer separately.  With ST9 MP1 and later we provided the Viewer .exe as part of the Solid Edge maintenance pack installation.  However, because of the nature of the MP technology, there is no way to provide a Start menu shortcut for the now provided ST9 Viewer.


With ST9 MP1 or later installed, you will need to manually create a shortcut for all users to the Solid Edge Viewer .exe file:


1. In "C:\ProgramData\Microsoft\Windows\Start Menu\Programs\Solid Edge ST9" create a new Shortcut.


2. Point the Shortcut to "C:\Program Files\Solid Edge ST9\Program\win32\seviewer.exe".


3. Name the Shortcut "Solid Edge Viewer ST9".


With ST9 MP1 and higher installed, following the above instructions will resolve the missing Viewer issue.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: INSIGHT_CONNECT
Version: V109.0
Function: FREE_VIEWER

Ref: 002-7008852

KB Article ID# PL7008852

Contents

SummaryDetails

Associated Components