Migrated SolidWorks drawings are not linked to the migrated SolidWorks files

2021-10-06T23:55:31Z

Summary


Details

When importing or migrating SolidWorks drawings into Solid Edge, the drawings are not linked to the migrated SolidWorks model files.



Solution

There are two caveats that must be considered when migrating SolidWorks drawings that you want linked to the SolidWorks models:


The units of the SolidWorks file must match the units of the Solid Edge template file.


The link between the original SolidWorks drawing file and model file must exist. The SolidWorks drawing cannot be saved as a "Detached Drawing".


If either of these points is not true, then the migrated SolidWorks drawing will *not* be linked to the migrated SolidWorks model.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: TRANSLATORS
Version: V219.0
Function: SW

Ref: 002-7008850

KB Article ID# PL7008850

Contents

SummaryDetails

Associated Components