Is it possible to install multiple Solid Edge languages on to the same system such that there is a multi-lingual Solid Edge environment available to the end user?
Solution
Currently Solid Edge only supports a bi-lingual setup - English and the native operating system language (if supported).
There is no supported method to allow running Solid Edge in another language other than English or the current operating system language. Therefore Solid Edge cannot be configured to provide a multi-lingual environment.
Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: L10N
Version: V219.0
Function: OTHER
Ref: 002-7008847