Details
Changing values in 'Occurrence Properties' will not work for some parts.
User can change and close 'Occurrence Properties', but previous values will be
kept and are shown if 'Occurrence Properties' is opened again.
Solution
Try the following workaround:
For example changing 'Draft Reference' for one part from 'Yes' to 'No'.
1. Enter 'Occurrence Properties'.
2. Change the corresponding field from 'Yes' to 'No' and press 'Apply'.
3. Change field back from 'No' to 'Yes' and press 'Apply'.
4. Finally change field from 'Yes' to 'No' again and 'OK'.
If you want to do changes for multiple parts, you can use this workaround by
selecting them together.
Notes and References
PR#7921705
Hardware/Software Configuration
Platform: INTEL
OS: window
OS Version: 864
Product: SOLID_EDGE
Application: ASSEMBLY
Function: COMPONENTS
Ref: 002-7008846