Call "User.dpv" files on network via startup script

2021-10-06T23:27:14Z

Summary


Details

--------------- 
Users have their own specific Customer Defaults file, they want these files to be on a network location via their Roaming profile and use them on starting NX.



Solution

For this you need to store each "NX100_user.dpv" file of each user on a network location with their logon name included, e.g. X:\NX_Userfiles\John\, X:\NX_Userfiles\Paul\, ...


In the NX startup script you then can refer to the logged on user, via %username%, which will collect the Windows user that is logged on, and set the variable :


 NX_USER_DIR X:\NX_Userfiles\


Then use this value to set the user specific *.dpv file in the UGII_LOCAL_USER_DEFAULTS variable.


When user "John" is logged on in Windows something like :


 UGII_LOCAL_USER_DEFAULTS=${NX_USER_DIR}\${USERNAME}\NX100_user.dpv


should result in --> X:\NX_Userfiles\John\NX100_user.dpv


Then the user specific Customer Defaults file is loaded when NX starts.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: GATEWAY
Version: V10.0
Function: CUSTOMER_DEFS

Ref: 002-7008842

KB Article ID# PL7008842

Contents

SummaryDetails

Associated Components