Holes missing in flat pattern of helical sheet metal part

2021-10-06T23:55:27Z

Summary


Details

The user has a Sheet Metal part which looks like a helix with holes along the 
whole length. After 360° the holes are lost in the flattened part.



Solution

Unfortunately Solid Edge often has problems with flanges/features exceeding 
360°. Consequently Solid Edge loses the holes which are positioned after the 
first "round" of the flange. Unfortunately Solid Edge will not allow you to 
create a pattern in the flattened part, however a workaround is still 
available.


The trick is to create a second part, which will be used as the flattened 
model.


1. Open the part in question. 
2. "Save As" -> and define a name e.g. flattened.psm (this will be the part to 
be used as flattened model). 
3. Unbend the model, using the edge nearest to the holes as a base. 
4. Now simply move the Unbend feature to directly before the Pattern of the 
holes. The Pattern should automatically find the "straight" edge instead of the 
helical edge, then update the hole pattern.


This should now show a flattened model with all holes. Use this model for 
further processing.



Notes and References

PR#7903760



Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 864
Product: SOLID_EDGE
Application: PART/SHEETMETAL
Function: FLAT_PATTERN

Ref: 002-7008829

KB Article ID# PL7008829

Contents

SummaryDetails

Associated Components