Export of an assembly to STEP format fails because of part/s

2021-10-06T23:55:01Z

Summary


Details

--------------- 
The export of an assembly to STEP format fails with a file translation error 
e.g. "x.asm could not be saved because of a file translation error."



Solution

One possible cause of this error message might be part/s inside the assembly 
that cannot be translated for any reason. Unfortunately, the STEP translation 
does not give more information about which file/s cannot be translated. Here is 
a tip how to find out.


Start 'Batch.exe' inside '...Program Files\Solid Edge ST9\Custom\Batch\Bin' 
folder and choose to translate all files in the folder to convert to STEP, the 
batch process translates one file after the other and stops with the message 
"y.par could not be saved because of a file translation error." and leaves the 
file open. If you then click OK to continue translation, the batch process 
would stop at any occurrence that shows this error and leave the file open.


At the end you would know which part/s hinder the translation process.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: SOLID_EDGE
Application: TRANSLATORS
Function: STEP

Ref: 002-7008645

KB Article ID# PL7008645

Contents

SummaryDetails

Associated Components