Solid Edge Ordered Cutout will stop if dynamically preview is OFF

2021-10-06T23:55:34Z
PART/SHEETMETAL

Summary


Details

If Solid Edge Options -> View 'Dynamically preview feature creation' is turned 
OFF, then subsequently when creating an ordered cutout the process will stop. 
After showing the direction of the cutout, the command will not proceed to the 
next step ('Finish'). All following buttons will be grayed out.



Solution

Turn 'Dynamically preview feature creation' ON. Doing this whilst creating the 
Cutout feature will cause the feature to be lost. Instead use 'CTRL+SHIFT+D' to 
turn on 'Dynamically preview feature creation' temporarily.



Notes and References

PR#7858006



Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 864
Product: SOLID_EDGE
Application: PART/SHEETMETAL
Function: FEATURES

Ref: 002-7008631

KB Article ID# PL7008631

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FLAT_PATTERN