Solid Edge Error occurs when migrating Solid Works files to Solid Edge

2021-10-06T23:55:26Z
TRANSLATORS

Summary


Details

When trying migrate Solid Works files to Solid Edge, getting an unknown error 
message.



Solution

 To use the migration tool without the DCOM Application the following needs to 
be done: 

-Install both Solid Works and Solid Edge on the same machine 

-You do not have to create a network share for the Solid Works files. A local 
folder is all that is necessary. 

-Do not install the Data Migration application from your Solid Edge install 
media. If you have already installed the Data Migration application, uninstall 
it, along with any files and/or folders the Data Migration application may have 
left behind after the uninstall. If the Data Migration application is not 
detected, the files will be processed in local mode. 

-Complete the fields in the dialog just as you have in the past, including the 
node name.



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 10_1909
Product: SOLID_EDGE
Application: TRANSLATORS
Version: V219MP9
Function: SW

Ref: 002-7008607

KB Article ID# PL7008607

Contents

SummaryDetails

Associated Components

TRANSLATORS: OTHER