---------------
Starting NX10, a Text feature can be used in a user defined feature
Solution
If you use file export user defined feature from a part containing a Text
Feature, and select it in the wizard, the chain expression will then be
available for selection.
Keep in mind that since it is a chain expression, when using the UDF, you will
have to keep this same syntax with the quotation marks "TEXT"
Notes and References
Hardware/Software Configuration
Platform: all
OS: all
OS Version: ALL
Product: NX
Application: DESIGN
Function: FEATURE_MODEL
Ref: 002-7008596