This part is now converted to use the new Iray+ Ray Traced studio rend

2021-10-06T23:27:11Z

Summary


Details

--------------- 
You may see the following information message opening a part file in NX 11.0: 
This part is now converted to use the new Iray+ Ray Traced studio rendering 
which produces the best rendering results. 
Any System Materials found in this part are converted to the new Iray+ 
materials



Solution

 In NX11 we introduced a new High End Visualization rendering engine 
(Iray rendering) which requires new materials. 
So upon loading the part, we convert all legacy materials 
to the new material types as much as possible. 
The materials that will be converted are those with names matching the ones in 
the NX11 System Materials palette. 
All other are converted to using the image with green Iray+ logo on it - to 
indicate to users that they have to reapply new Iray+ materials. 


If you don't want to convert you can set the variable NX_RTS_IRAY=0



Notes and References


Hardware/Software Configuration

Platform: all
OS: all
OS Version: ALL
Product: NX
Application: SYSENG
Function: VISUALIZATION

Ref: 002-7008595

KB Article ID# PL7008595

Contents

SummaryDetails

Associated Components