---------------
When using ugmig.exe utility in NX11.0 it will only generate
black and white images
For example :
Start a NX10 command prompt and type in the following:
D:\SIEMENS\NX 10.0\UGMANAGER>ugimg -f tif F:\SUPPORT\NX10.prt
The resulting NX10.tif file is colored
Start a NX11 command prompt and type in the following:
D:\SIEMENS\NX 11.0\UGMANAGER>ugimg -f tif F:\SUPPORT\NX11.prt
The resulting NX11.tif file is gray
Solution
First of all this is fixed in NX 11.0.1
Nevertheless, Please note that batch shading is not supported in the new Iray
Mode as specified in the documentation for uf_disp.h.
Please set NX_RTS_IRAY=0 before running ugimg utility.
Notes and References
Hardware/Software Configuration
Platform: all
OS: all
OS Version: ALL
Product: NX
Application: GATEWAY
Function: PLOTTING
Ref: 002-7008594