Tecnomatix Encrypt XML files for Process Simulate

2021-10-07T00:01:33Z
Process Simulate

Summary


Details

I have a working custom XML file and want to be sure that nobody will edit or change it. What do I do?



Solution

There is an encryption mechanism built into Process Simulate. See Chapter One of RoboticsCustomizedUIManual.pdf under "eMPower\Help\Additional Reference Material". From inside the "Customized Commands XML Checker" window, there is a button you can click on called "Encrypt".


To protect customized XML files, it is possible to use encryption. To do so, select the Encrypt button and select the XML files to encrypt. The encrypted files are created with the XMLC suffix and can be safely shipped to contractors and suppliers. Process Simulate handles both XML and XMLC files transparently.



Notes and References


Hardware/Software Configuration

Platform: na
OS: n/a
OS Version: n/a
Product: TECNOMATIX
Application: PROCESS_SIMULAT
Version: V14.1
Function: CUSTOM_APPLICAT

Ref: 002-7008573

KB Article ID# PL7008573

Contents

SummaryDetails

Associated Components

Process Simulate API Development