---------------
Is there a quick way to inherit annotation style settings from existing dimensions and PMI in NX?
Solution
NX has added a new option on the MB3 shortcut menu called "Inherit". While creating or editing a dimension use
MB3--> Inherit and then select the existing dimension or PMI to inherit the display style
from.
This action will also inherit any appended text associated with the selected dimension or PMI.

In the Dimension dialog Settings area you will still find the "Select Dimension to Inherit" option but it will use the new icon design.
Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 1064
Product: NX
Application: DRAFTING
Version: V1847
Function: ANNOTATION
Ref: 002-7008426