Solid Edge Cannot register ISOtable as custom bend formula

2021-10-06T23:55:02Z
PART/SHEETMETAL

Summary


Details

Registering a custom bend formula is not working. When applying the custom 
formula will show an error stating "bend equation Automation object is not 
registered. Using neutral factor settings". This also happens when using the 
default ISOtable in the custom folder.



Solution

Using the examples in C:\Program Files\Solid Edge 
ST*\Custom\sheetmetal\ISOTable\bin\


and using "Register.bat" in the same folder will cause this problem.


Looking at "Register.bat":


%SystemRoot%\Microsoft.NET\Framework64\v4.0.30319\regasm /codebase 
bin\ISOTable.dll 
%SystemRoot%\Microsoft.NET\Framework64\v4.0.30319\regasm /tlb bin\ISOTable.dll


This will show a wrong path to ISOTable.dll. You have to delete "bin\" in both 
lines. Then registering will work, and applying the formula in Solid Edge will 
also work. The same applies in "UnRegister.bat"


Alternatively you can use "RegisterSample.exe", which interactively asks you to 
register or unregister.



Notes and References

IR#7728775



Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 864
Product: SOLID_EDGE
Application: PART/SHEETMETAL
Function: FLAT_PATTERN

Ref: 002-7008411

KB Article ID# PL7008411

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FLAT_PATTERN