NX What Are The Benefits Of Saving A Bookmark In Clearance Analysis?

2021-10-06T23:26:53Z
NX for Design

Summary


Details

Clearance Analysis has the ability to Save Bookmark. What information is saved in the bookmark?



Solution

The Clearance Analysis bookmark saves the assembly context including component visibility, load options and component groups.


The bookmark also saves the state of the Clearance Browser. It stores which clearance set you're looking at and which interference boxes were checked when the bookmark was saved. Component positions are not saved.


At the bottom of the Save Bookmark dialog is a "Record" drop down list where the user can choose how much information is saved. The options are: 


  • Component Groups, Options, Structure and Display Settings
  • Component Groups, Options & Structure 
  • Component Groups & Load Options 
  • Component Groups Only



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: ASSEMBLIES
Version: V1847
Function: ASSEMBLY_MODEL

Ref: 002-7008390

KB Article ID# PL7008390

Contents

SummaryDetails

Associated Components

Assemblies