Resizing the dynamic WCS

2021-10-06T23:26:54Z

Summary


Details

Having made several changes to NX it was found that the Dynamic WCS was very small when using the Move Object command, however, the user could not recall which setting caused the change.



Solution

The size of the Dynamic WCS can be controlled using the Visualization Preferences.


Select "File --> Preferences --> Visualization" and select Calibration from the menu on the left of the dialog.  Select "Reset to System Defaults" and then Apply to restore the Dynamic WCS to the default size.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: GATEWAY
Version: V1847
Function: PREFERENCES

Ref: 002-7008388

KB Article ID# PL7008388

Contents

SummaryDetails

Associated Components