Preventing The On-Context Toolbar Displaying When Selecting Points in NX

2021-10-06T23:27:06Z

Summary


Details

A popup toolbar is displayed whenever a point is selected in the NX graphics display.  How can this be disabled?



Solution

  1. Select "Menu --> Tools --> Customize" and select the Commands tab

  2. Select an existing point in the graphics display which opens two toolbars

  3. Drag the icons on the toolbars into the Commands window to remove them from the popups until none are left

  4. Close the Customize dialog.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: DESIGN
Version: V1847
Function: CURVE

Ref: 002-7008382

KB Article ID# PL7008382

Contents

SummaryDetails

Associated Components