NX Using ug_clone.exe desc of specification disappears in export.clone

2021-10-06T23:26:54Z
NX for Design

Summary


Details

--------------- 
Using USE_EXISTING in export.clone file and export the description of the prt 
file of 2D disappears in export.clone file.


(1)Make the export.clone file of the condition to export 2D and 3D. 
¦&LOG Default_Cloning_Action: USE_EXISTING 
(2)Carry out ug_clone.exe and export prt file of 3D, prt file of 2D to a local 
PC. 
(3)Confirm updated export.clone file. There is the description of the prt file 
of 2D and 3D. 
(4)Make the export.clone file of the condition same as procedure (1). 
¦&LOG Default_Cloning_Action: USE_EXISTING 
(5)Carry out ug_clone.exe and export prt file of 3D, prt file of 2D to a local 
PC. 
(It is identical to 2 procedures.) 
(6)Confirm updated export.clone file. There is no description of the prt file 
of 2D.



Solution

 If the UGMASTER is not exported then any non-master parts under the same 
ItemRevision are not exported. There is no guarantee that the version of the 
master on the OS corresponds to version in the database.



Notes and References

IR/PR 7659489



Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 764sp1
Product: NX
Application: NXMANAGER
Version: V8.5.3
Function: CLONE

Ref: 002-7008357

KB Article ID# PL7008357

Contents

SummaryDetails

Associated Components

Teamcenter Integration for NX