'Move Object' will not select objects from model space in drafting app

2021-10-06T23:26:57Z

Summary


Details

--------------- 
'Move Objects' does not select modeling objects in the Drafting Application 
when the Drawing display Off.


NX was able to do this in the NX5 & previous version 'Transform' operations.



Solution

 From NX6 the 'Move Objects' does not select modeling objects in the Drafting 
Application when the Drawing display Off is working As Designed. 
When the Application is Drafting, only objects that were created in Drafting 
Application are allowed for transformation with Move Object. Because of this 
behavior, the curves present in assembly part/model part are not selectable 
when sheet display is 'off' while they are selectable if the application is 
changed to Modeling.



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 764
Product: NX
Application: DRAFTING
Function: MOVE_OBJECT

Ref: 002-7008343

KB Article ID# PL7008343

Contents

SummaryDetails

Associated Components