---------------
Suppose user has deleted some of the directories from the NX installation
directories. Now user is worried if he will be able to run the NX uninstall
wizard correctly so that the NX will be uninstalled cleanly. User wants to
know that are some directories of NX installation required to run the NX
uninstall wizard.
Solution
None of the directories are necessary to run the NX uninstall. The NX
uninstall runs the MSI that windows cached when the product was installed,
and references nothing in the directories.
Notes and References
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: SYSENG
Version: V10.0.3
Function: INSTALL_ISSUES
Ref: 002-7008291