About "Tracking Bar" of 'Basic Curves'.

2021-10-06T23:26:49Z

Summary


Details

--------------- 
"Tracking Bar" is not shown when started 'Basic Curves' dialog in NX10.



Solution

 The "Tracking Bar" if either closed or has slid off the screen, then it will 
not be shown up when you start 'Basic Curves' dialog. 
You can show the "Tracking Bar" by either of the following ways: 
1. With the Basic Curve dialog open, select Preferences --> User Interface -- 
> Cancel. If the tracking bar was closed, this will reopen it. 
2. With the Basic Curve dialog open, select Preferences --> User Interface -- 
> Layout tab --> Reset Window Position icon.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V10.0.3
Function: CURVE

Ref: 002-7008286

KB Article ID# PL7008286

Contents

SummaryDetails

Associated Components