Simcenter 3D Solutions "Use Element Associated Data" for 1-D and 2-D elements

2021-10-06T23:27:04Z
Simcenter 3D

Summary


Details

--------------- 

The mesh associated data of 2D elements has "Use Element Associated Data" 

button. 

Why doesn't 1D element have "Use Element Associated Data" button?

Solution

 The switch is simply a "use or ignore" type of switch.

If the switch is ON, then the exporters will use the element associated data 

(where it exists). If the switch is OFF, then all element associated data is 

ignored and only the mesh associated data is used. The switch doesn't exist for 

1D meshes because 1D mesh associated data tends to produce element associated 

data anyway.

Notes

KB Article ID# PL7008257

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow