Simcenter 3D Solutions Remove the exponent of the coordinate values of Grid while exporting

2021-10-06T23:26:47Z
Simcenter 3D

Summary


Details

--------------- 

How to remove the exponent(E+00) of the coordinate values of Grid while 

exporting?

Solution

 If you toggle off “Performance Mode” in the Advanced Solver Options and set the 

Field Length to “Large” 

You will get the following format which does not contain the “E”

GRID* 8 0 100.0 100.0+ 

* 100.0 0

The exponential notation will be used only when needed. However, the formatting 

settings apply to the whole deck, not just the GRID.

Notes

KB Article ID# PL7008255

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow