---------------
In simulation with time increment, we want to output the field of stress change
with the time in certain element (which is feasible in ABAQUS CAE with history
output requests).
How to do this in NX CAE?
Solution
NX can output both the Field and History output simultaneously, but cannot
control output requests independently.
1. Click Modeling Objects icon.
2. Set Type as "Abaqus Structural output Requests" in Modeling Objects Manager
dialog box, then click Create button.
3. In Abaqus Structural Output Requests box, Check the Written into ODB file
button,then select "Field and History" for Field/History option.
4.Please note you cannot set different requests for each Field/History options
Notes
7752548