Simcenter 3D Solutions Can IDEAS ESC + IDEAS TMG Radiation migration to NX use Thermo-Optical properties-Advanced.

2021-10-06T23:27:17Z
Simcenter 3D

Summary


Details

--------------- 

Can IDEAS ESC + IDEAS TMG Radiation migration to NX use Thermo-Optical 

Properties-Advanced?

Solution

 For the optical properties. There are 2 types of modeling objects: 

1. Thermo-Optical Properties 

2. Thermo-Optical Properties-Advanced 

Type 1 can be used with just NX ESC License 

Type 2 can be used with NX ESC + NX Advanced Thermal license.

The default migration path from IDEAS ESC + IDEAS TMG Radiation would be NX ESC 

+ NX Advanced Thermal.

So Thermo-Optical Properties-Advanced can be used upon migration.

Notes

7760716

KB Article ID# PL7008251

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow