Must repoint software to the license file after each reboot.

2021-10-07T00:01:43Z

Summary


Details

Each time user logs into workstation after a reboot, he must repoint the Plant Simulation software to the license file.



Solution

When you point PlantSimulation at the license it modifies the registry. The most likely issue is that the user does not have permissions to modify the registry. Hence it is changed only temporarily. The other possibility is that the OS is set up to restore values in the registry.


1. Point Plant Simulation at the license 

2. Run regedit and check HKEY_CURRENT_USER\Software\Tecnomatix\Tecnomatix Plant Simulation 13.0\Preferences\LicenseFile 

3. Reboot 

4. Run regedit and check HKEY_CURRENT_USER\Software\Tecnomatix\Tecnomatix Plant Simulation 13.0\Preferences\LicenseFile


It should be pointed at PLMLicenseServer\splm8.lic both times.



Notes and References


Hardware/Software Configuration

Platform: na
OS: n/a
OS Version: n/a
Product: TECNOMATIX
Application: PLANTSIMULATION
Version: V13.0
Function: LICENSING

Ref: 002-7008177

KB Article ID# PL7008177

Contents

SummaryDetails

Associated Components